Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What frequency is the internal oscillator in Tiny series of devices ?

Latest Updated:03/26/2009

Question:

What is the frequency of the internal oscillator in the Tiny series of devices ?

Answer:

The frequency is not defined, the manual defines the minimum on chip overflow time and states a typical overflow period.
Suitable Products
H8/300H Tiny