Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What happens if the time for supply voltage exceeds specified value?

Latest Updated:10/11/2007

Question:

(Reset)  What will happen if the time for the supply voltage to rise from 0V to the minimum voltage for recommended operating conditions exceeds the specified value? [2007/10/11]

Answer:

If internal reset signal is released before the supply voltage reaches the minimum voltage for recommended operating conditions, reset may fail. (#106772)
Suitable Products
4286