Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is difference between temperature code D and P in the part number?

Latest Updated:03/29/2013

Question:

What is difference between temperature code "D" and "P" in the part number?

Answer:

Make sure to be aware of the following difference when ordering:
D version: standard quality version (-40 degrees C to 85 degrees C)
P version: high quality version (-40 degrees C to 85 degrees C)
Suitable Products
R32C/116A, R32C/117A, R32C/118A
R32C/116, R32C/117, R32C/118