Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is oscillation stop detection circuit detection frequency mean?

Latest Updated:12/16/2004

Question:

(Clock)  What does the "oscillation stop detection circuit detection frequency" specification in Electrical Characteristics mean? [2004/12/16]

Answer:

The oscillation stop detection circuit monitors main clock oscillation frequency using the on-chip oscillator (standard: 2MHz).
Oscillation stop is detected when at least 4 clocks of the main clock have become slower than 1/16 of the on-chip oscillator (standard: 125kHz). (#104948)
Suitable Products
7544
7546
7547