Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the A/D conversion speed?

Latest Updated:02/14/2006

Question:

What is the A/D conversion speed?

Answer:

It is:
33 øAD cycles in 10-bit resolution with a sample & hold;
28 øAD cycles in 8-bit resolution with a sample & hold.
For example, it is 2.06µs for M32C/85 Group (øAD=16MHz, 10-bit resolution with a sample & hold) and 2.75µs for M16C/62P Group (øAD=12MHz, 10-bit resolution with a sample & hold).
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N