Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the differences between the R8C Family and the M16C/60 Series.t

Latest Updated:03/07/2012

Question:

I want to know the instruction set differences between the R8C Family and the M16C/60 Series.

Answer:

The R8C Family doesn't support JMPS and JSRS instructions. These instructions branch to the program set from F0000h to FFFFFh block number, but the R8C Family has no ROM in this area, so you can't use these.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A