Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the frequency of the system clock if WDT overflows?

Latest Updated:03/26/2009

Question:

If the internal oscillator is selected by watchdog timer (WDT), is the overflow time set to MIN0.2,TYP0.4SEC regardless of frequency of the system clock?

Answer:

With the internal oscillator, setting overflow time is made independently from the system clock and sub-clock. The time to the generation of internal reset by counting up from 0 to 255 is 0.2-typ0.4sec.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902