Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the oscillation settling time of the on-chip oscillator?

Latest Updated:05/24/2007

Question:

(Clock)  What is the oscillation settling time of the on-chip oscillator? [2007/05/24]

Answer:

When the MCU is used within the specified values, oscillation settling time is not required. (#106675)
Suitable Products
4508
4509
4559
455A