Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the value of TxD pin when TE bit of SCR is set to 1?

Latest Updated:03/26/2009

Question:

What is the initial value of TxD pin, when the TE bit of serial control register (SCR) is set to 1?

Answer:

When TE bit is set to 1, the initial value of TxD pin automatically takes on a high level in the asynchronous and clock synchronous modes. However, it is necessary to set to 1 the TXD bit of the port mode register before TE bit is set, when setting the TxD pin to output.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902