Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Will the WDT also resets if its full when the LSI resets internally?

Latest Updated:03/24/2009

Question:

The hardware manual states that if WDT overflows, the entire LSI is reset internally. In this case, is the WDT also reset?

Answer:

All functions except for WRST bit of TCSRW (Timer control/status resistor W) are reset. Initialization of WRST bit is performed by external reset pin, not by the overflowing of the WDT.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power