Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Difference between the version number and the revision number for a compiler

Last Updated:05/17/2017

Question:

What is the difference between the version number and revision number for a compiler?

Answer:

The version number is the numeral immediately after the “V”. This number is increased in cases of dramatic additions of functionality or major modifications to an MCU’s architecture. The revision number is the number which follows the version number. It is increased with each minor revision.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family