Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Differences between Sections .text, .textf, .const, and .constf_CC-RL

Last Updated:02/07/2018

Question:

I am using RL78 compiler CC-RL.
There are sections .text, .textf, .const, and .constf in the link map information. What are the differences among them?

Answer:

Sections .text and .textf are for code. The former is allocated to the near area and the latter to the far area.
Sections .const and .constf are for ROM data. The former is allocated to the near area and the latter to the far area.

For details on sections output by CC-RL, refer to the user’s manual below.

   CC-RL Compiler User’s Manual
     6. Section Specifications
 

Suitable Products

e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family