Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

E0562320 error message and the -rom option (CC-RL)

Last Updated:06/14/2017

Question:

I am using the RL78 CC-RL compiler. The section specified in the -rom option leads to the following error. How do I resolve this?

“E0562320: Section address overflowed out of range : "section""

Answer:

The -rom option of the linker can be specified in the following format.
 -rom=ROM section=RAM section [,ROM section=RAM section]...
The section indicated at the right of “=” should be allocated within the range of RAM.
See the hardware manual for the MCU you are using to check the address range of the on-chip RAM, then allocate “RAM section” in the -rom option in the on-chip RAM.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family