Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

F0563430 Message(CC-RL)

Last Updated:06/14/2017

Question:

I am using RL78 compiler CC-RL. How do I resolve the “F0563430: The total section size exceeded the limit” error?

Answer:

The error message appears when 60 or more days have passed since the first build for CC-RL V1.xx.xx and the evaluation period of the evaluation edition has expired, and also the size of linkable object has been over 64KB.

If you have the commercial edition of the compiler, register its license key via license manager.

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family