Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Professional Edition License Operates as Evaluation Edition_Floating License

Last Updated:12/13/2017

Question:

I am building an environment with a floating license. I have registered a license key of the professional edition in a server PC. When building in a client PC, I get a message which says the license is the evaluation edition. How do I resolve this?

In addition, when I acquire the license in offline mode, the message does not appear during building.
 

Answer:

For the floating license server administrator software, select the [Offer the upper-level license if lower-level license is empty.] checkbox in [Option].

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?