Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Setting the Floating License Server

Last Updated:12/13/2017

Question:

To use a floating license, do I need to set up the server PC to be accessed by other PCs?

Answer:

You need to set the port number and other settings necessary to enable communication. For details, refer to the user's manual below.

  Floating License Server V2.01.00 User's Manual
   2.3.1 Setting up the server
   2.3.2 Setting up the firewall
 

Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family
  • Was this article helpful?