Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Settings of Floating License Server in Web Server

Last Updated:12/20/2017

Question:

In the case of using floating license server software in a Web server PC, are there any cautions to be considered?

Answer:

To use a floating license, you need to set the port number and other settings to enable communication. In this case, do not specify the port numbers that are assigned for services.
Suitable Products
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family