Skip to main content
Renesas Electronics America - Knowledgebase

Stack smashing detection function in the professional edition (CC-RL)

Last Updated:05/10/2017


I am using RL78 Compiler CC-RL.
Is the stack smashing detection function, the additional function of the professional edition, able to work (perform a detection) only for debugging?


The stack smashing detection function generates codes that can detect stack smashing, and can be used for other than debugging.
You can find the usage examples of the stack smashing detection function in the following document:

- Compiler CC-RL User's Manual
 2.5.1 Compile options
  Code generation changing

Suitable Products
e² studio
CS+ (formerly CubeSuite+)
C Compiler Package for RL78 Family