Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Using Standard Library Function_CC-RX

Last Updated:03/20/2018

Question:

I am using RX Compiler CC-RX.
When including the header file math.h for using the standard library function cosf(), the following error message appeared.

E0562310 Undefined external symbol "symbol" referenced in "file"

Answer:

To use standard library functions in CC-RX, you need to add #include in a source file and specify the [Library Generate Options] settings.

Select the [Library Generate Options] tab in the CC-RX (build tool) property dialog on CS+ >> [Standard Library] >> select [Yes] for [Enables math.h(C89/C99)], then execute building.
For using single-precision operations for all data, select mathf.h. For double-precision operations, select math.h.

If the same error occurs with the other standard library functions, you can resolve it by enabling the necessary standard library.
 

Related FAQ:

Description about inclusion of the header file in the standard library (CC-RL)

What to do if the expected result of standard CC-RX is not obtained?

Suitable Products
C/C++ Compiler Package for RX Family