Which should I use if I have both a node-locked and floating license installed on the same PC?
Question:
Answer:
Enabling or disabling the floating license can be selected.
When enabling, use the license in the following manner:
1. When either the node-locked license or the floating license is a professional version:
The professional license takes precedence.
1.1
When the node-locked license is a professional version
and the floating license is a standard version:
Use the node-locked license.
1.2
When the node-locked license is a standard version
and the floating license is a professional version:
Use the floating license.
1.3
When both licenses are professional versions:
Use the node-locked license.
2. When both the node-locked license and the floating license are standard versions:
2.1
In case of CC-RH V1.05.00/CC-RX V2.06.00/CC-RL V1.04.00:
Use the node-locked license.
2.2
In case of a revision earlier than 2.1:
Use the floating license.
C Compiler Package for RH850 Family |
C/C++ Compiler Package for RX Family |
C Compiler Package for RL78 Family |