Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Debugging flexible exception handling when using on-chip debugging emulator (serial)

Last Updated:03/22/2017

Question:

An on-chip debugging emulator (serial) doesn’t return response.

Answer:

When a serial OCD interface (debugging through a UART/CSI) is in use, the user must handle communications between an emulator and the target device by programming the debugging monitor program into the exception handler.
Therefore, the switched exception handler address may cause a communication error between the target device and the emulator.
For flexible exception handling, use an emulator which supports JTAG connection.

emulator which supports JTAG connection

V850E2
E1(JTAG)
E20(JTAG)
QB-V850MINIL
Suitable Products
 
V850E2
E1(Serial)
E20(Serial)
MINICUBE2
E1(JTAG)
E20(JTAG)
QB-V850MINIL