Skip to main content
Renesas Electronics America - Knowledgebase

Error message: downloading program to 78Ko in E1 or E20 from CubeSuite+

Latest Updated:10/24/2014


When I downloaded a program to the 78K0 family microcontroller through the E1 or E20 from CubeSuite+, the following error message appeared.

Error (E0210002)
Launching debugger failed.

[Direct Cause of the Error]
Illegal condition. (E1201024)


This is due to the setting of [Main clock source] for [Clock] on the [Connect Settings] tabbed page of the debug tool for CubeSuite+ being "Clock board", which is the initial value.
Set [Main clock source] as "Generate by emulator".
Suitable Products
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]