Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How to create a project and the specification of debugging function?

Latest Updated:10/15/2014

Question:

I would like to know the way of creating a project and the specification of the debugging function when a multi-core device in the RH850 family is used.

Answer:

Please see the following documents:

Note that the documents are for the multi-project and one for the single-project is in the making.

Tutorial for RH850 Multi core (Debug): r20ut3068
Overview of Programming for RH850 Multi-core: r20ut3069
Tutorial for RH850 Multi-core (Build): r20ut3070

Suitable Products
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]