Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How to download a file to the debug tool in CubeSuite+, without errors?

Latest Updated:09/30/2014

Question:

When attempting to download a file to the debug tool in CubeSuite+, "Download failed. [Direct Error Cause] Can not open file. (E1249153)" is displayed.

Answer:

A load module of the active project is to be downloaded.
Confirm whether the target project is active.
Also confirm that you are not attempting to download a load module of an unbuilt active project.
Suitable Products
E1 [R0E000010KCE00]