How to install emulator control program without CD-ROM
Last Updated:09/27/2017
Question:
I have lost the CD-ROM that came with the emulator when I purchased it. How can I install the emulator without the CD-ROM?
Answer:
The emulator software, trial version compiler and other tools included on the CD-ROM can be downloaded from the following site.
https://www.renesas.com/search/keyword-search.html#genre=tooldownload
On the left side of the screen, select [Software and Tools] → [Emulation and Debugging], and download the necessary emulator control program.
Suitable Products
E1[R0E000010KCE00] |
E20[R0E000200KCT00] |
E10A-USB |
E8a |
E10T-USB |
E8 |
E100 |
E200F |
E6000H |
PC7501 |