Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

I don’t know the ID code when I turn on E1 or E20.

Last Updated:01/31/2018

Question:

When I turn on E1 or E20 (using with an RX Family MCU), the ID code confirmation dialog box is displayed, but I don’t know the ID code and can’t complete the connection. Is there a workaround in this case?

Answer:

The ID code is an MCU function that prevents a third party from illegally acquiring the contents of the flash memory.
The ID code is written in the ROM (flash memory for code storage) of the RX Family MCU. If you know which program (MOT or ABS file) you downloaded to the target MCU, you can obtain the ID code by reading the address of the program download with a simulator, etc.

For more information on the ID code address, refer to the explanation of “ID Code Protection” in the corresponding MCU hardware manual. (RX610 Group: section 26.10.2; RX62N Group: section 37.9.2; RX62T Group: section 30.9.2)

If you are unsure of which program you downloaded to the target MCU, you will not be able to obtain the ID code. In this case, you will need to clear the flash memory using the boot mode. However, even in this solution, depending on the control code value for the ID code (see the MCU hardware manual for more info.) you may not be able to clear the flash memory. If this is the case, the only solution is to replace the MCU.

Renesas also offers a Flash Development Toolkit for use in the boot mode. Download the trial version (free of charge) from here.

Note: For RX610 Group MCUs, the communication method used in the boot mode and used with an on-chip debugging emulator is different.
Please refer to the corresponding communication method as follows:

  • When using the RX610 Group with the on-chip debugging simulator
    Refer to “2. Connecting the Emulator with the User System” in the  manual for RX610 group.
  • When using RX610 in the boot mode:
    Refer to Connection examples (E1/ E20 emulator) of RX610 Group from here.
Suitable Products
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]