Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

List of error messages when using E1/E20 emulator in CS+

Last Updated:04/26/2017

Question:

List of error messages when using the E1/E20 emulator in the CS+ environment

Answer:

When the following error messages are displayed, refer to the FAQ below.

The limitations of E1/E20 differ depending on the MCU used in your systems. Please confirm each item of [Notes on Using the E1/E20 Emulator] on the [E1/E20 Emulator Additional Document for User's Manual] to find a solution for your case.
You can download [E1/E20 Emulator Additional Document for User's Manual] from here.

Timing of occurrence Suitable MCU Error Message FAQ No
At start up/ connection RX Error (E0210002) Lanching debugger failed
[Direct Error Cause]
A timeout error. The MCU is in the reset state. (E1814001)
RL78 Error (E0210002) Lanching debugger failed
[Direct Error Cause]
The ID code is incorrect. (C0602202)

Executing program failed
[Direct Error Cause]
No response from the CPU. Please confirm the signal of the CLOCK or RESET and so on.

Download failed.
[Direct Error Cause]
No response from the CPU. Please confirm the signal of the CLOCK or RESET,WAIT and so on.(E1200416)

1010241

1010535

Download failed.
[Direct Error Cause]
Unable to connect to the emulator (xxx). (E1899000)
1010196
Refer to the answer of the FAQ.1010196 for the solution to this error.
V850 Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
Incorrect ID Code.(C0602202)
Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
DCU cannot be accessed.(E1203184)
Monitor memory cannot be accessed.(E1203186)
RH850 Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
Incorrect ID Code.(C0602202)
Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
Failed in connect. Please check the connection of the emulator and target.(E1203237)
Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
DCU cannot be accessed.(E1203184)
V850,RH850 Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
Target power mode mismatch.(E1202820)
Error(E0210002) Launching debugger failed.
Error(E0204001) Download failed.
[Direct Error Cause]
Guarded area can not be accessed.(E1203104)
At write/
download
RL78 Download failed
[Direct Error Cause]
Writing to the on-chip debug reserved area is prohibited (address:0x****) (E1203124)
RX An error has occurred in verification of the external flash ROM. The flash ROM may have been degraded. (E1812802)
An error has occurred in erasing of the external flash ROM. The flash ROM may have been degraded. (E1812800)
1010789
An error has occurred in programming of the external flash ROM. The flash ROM may have been degraded. (E1812801) 1010790
Programming of the on-chip ROM area is not available during execution of the user program. (E1811301) 1010791
RX,RL78 Download failed.
[Direct Error Cause]
Can not open file. (E1249153)
1011178
78K
Error (E0210002) Launching debugger failed.
[Direct Cause of the Error]
Illegal condition. (E1201024)
1011216
Error (E0204001) Download failed.
[Direct Cause of the Error]
Writing to the on-chip debug reserved area is prohibited. (address:0x190) (E1203124)
1011218
Debugging RL78 Executing program failed.
[Direct Error Cause]
No responce from the CPU. Please confirm the signal of the CLOCK or RESET and so on.
RX Because the access violation etc. to on-chip ROM area are generated, the flash rewriting cannot be executed.(E1811307)
RX, RL78 “An error has occurred during the communication with the emulator(FFWERR_COM). Disconnect the debugger and reconnect the USB cable. Then turn on the power of the emulator and initiate the debugger."
Suitable Products
CS+ (formerly CubeSuite+)
E1 [R0E000010KCE00]
E20 [R0E000200KCT00]