What are the differences of HS0005KCU01H and HS0005KCU02H?
Latest Updated:03/14/2011
Question:
What are the functional differences of E10A-USB emulators HS0005KCU01H (no AUD function) and HS0005KCU02H (with AUD function)?
Answer:
The HS0005KCU02H (with AUD function) offers a more enhanced trace function compared to that of HS0005KCU01H (no AUD function). (Enhanced functions vary according to MCU)
For details on the AUD Trace, click here for a list of major debugging functions.
For details on the AUD Trace, click here for a list of major debugging functions.
Suitable Products
E10A-USB |