Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

In some cases, "acre_tsk" may return "E_NOID" after "exd_tsk" is called. Why?

Last Updated:05/17/2017

Question:

The E_NOID (No ID available) error may be returned when “acre_tsk” (Create task and assign task ID automatically) is called after the execution of “exd_tsk” (Exit current task and delete it).  What does this mean?

Answer:

This error can occur for the following reasons:
1. The service call “exd_tsk” has not been executed.  
When a task ends, "exd_tsk" is normally called. Therefore, the task ID is not returned and becomes unavailable.

2. “ext_tsk” has been coded, not “exd_tsk.”

3. On the HI7000/4, the target ID of “acre_tsk” (Create task and assign task ID automatically) is “CFG_STSTKID+1 to the maximum ID”, not “1 to the maximum ID.” “1 to CFG_STSTKID” is a task using static stack. Therefore, even when “exd_tsk” is called for the task, “acre_tsk” may not be applied.

 

Suitable Products
HI7000/4 Real-time OS for SuperH Family