Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Simulator stops with the INT instruction

Last Updated:05/17/2017

Question:

When debugging is done using a simulator, why does it stop when the INT instruction is executed?

Answer:

This is a simulator setting issue. Since the default setting of the simulator is “stops with the INT instruction exception,” you may need to change it. In the RI600V4 sample project, it has been set to not stop with the INT instruction.
Suitable Products
RI600V4