Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Why is the value of an event flag cleared after an event occurs?

Last Updated:05/17/2017

Question:

Why is the value of an event flag cleared after the corresponding event of the event flag occurs?

Answer:

If "TS_CLR" is specified as the attribute of an event flag, then the value of an event flag is cleared after the corresponding event occurs.

 

Suitable Products
HI7000/4 Real-time OS for SuperH Family