Skip to main content
Renesas Electronics America - Knowledgebase

Applilet2 does not work on Windows 7

Last Updated:08/02/2017


After I migrated from Windows XP to Windows 7, Appliet2 for xx does not work.


Applilet2 creates temp files for operation in the Program Files folder of Windows. Since writing in the Program Files folder is prohibited in Windows 7 and later, Applilet2 does not work. Search by “windows 7 programfiles authority”, and change the administrator authority of the Program Files\NEC Electronics Tools folder or below, then change to the log-on user.
Suitable Products
Code Generator