Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Does the CPU of a PC work in a multiprocessor environment?

Latest Updated:12/01/2011

Question:

I'm using the CA850 development environment on Windows NT 4.0.
Does the CPU of a PC work in a multiprocessor environment?

Answer:

The CPU of a PC may work even in a multiprocessor environment.
However, an improvement in the performance cannot be expected because use of multiprocessors is not valid according to the specifications.
Suitable Products