Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Error Message: C3304 (F) Cannot delete internal file

Latest Updated:02/18/2013

Question:

The following compile error occurs in building.

C3304 (F) Cannot delete internal file

Answer:

This error is output when an intermediate file created by the compiler cannot be deleted.
The following should be confirmed.

  • The error may be generated by the realtime search of an antivirus software.
    Temporarily disable the realtime search of the antivirus software during building.

  • Specify a location with a slow access speed (e.g., network drive) as the destination for setting SHC_TMP.

  • Execute a build using administrative authority.

Also refer to the FAQ below because the error might be prevented by the method described in the FAQ.
FAQ 106515

Suitable Products
C/C++ Compiler Package for SuperH Family