Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Error Message: W0070: Functions are treated as far function

Latest Updated:11/20/2014

Question:

I am using the RL78/78K0R compiler. I get the following warning message when I try to build a project.

W0070:Functions are treated as far function

Is there any countermeasure?

Answer:

This message will be inevitable if the x type is specified for the '-z' functional extension specifier for the output of objects for placement in RAM.
There is no way to suppress this message.
Suitable Products
C Compiler Package for RL78 and 78K Families
Compiler for RL78 Family and 78K0R [CA78K0R]
Compiler for 78K0R [CC78K0R]