Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How to compare the contents of the OTP-version file and the **.MSK file?

Latest Updated:09/15/2006

Question:

How can I compare the contents of the OTP-version file and the **.MSK file I created with the Maskfile converter.

Answer:

Unfortunately, you cannot compare the mask file and the OTP file because the mask file includes not only the hexadecimal data to be written to the MASK ROM, but also various data essential for performing the ROM mask process.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering