Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Will some info lost if I use compress linker option with debugging info?

Latest Updated:09/18/2015

Question:

Is any information lost if I use the –compress linker option to compress the debugging information?

Answer:

No information for use in debugging will be lost. Compressing shortens the loading time for the debugger and reduces file sizes while retaining the information needed for debugging.

Note, Linkage time and the memory usage during linkage can be increased relative to when the –nocompress option is specified.

Suitable Products
C/C++ Compiler Package for SuperH Family
C Compiler Package for RH850 Family
C/C++ Compiler Package for RX Family
C Compiler Package for RL78 Family