Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can AVG anti-virus software interfere with e2 studio and Synergy Software Package installation causing a toolchain failure?

Latest Updated:09/15/2016

Question:

I installed e2 studio and SSP but I can't start a Synergy Project. What could be the problem?

Answer:

If you have the AVG anti-virus running during the e2 studio and SSP install it can keep some of the installation from running. This results in an incomplete tool chain installation. The resulting tool chain fails to open Synergy Projects correctly. If you install e2 studio without the AVG software the tool chain is installed correctly.