Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can I Easily Install a Custom BSP or Pack into a Synergy Project?

Last Updated:02/15/2018

Question:

Is there an easy way to install a custom BSP or Pack into a Synergy project?

Answer:

Yes, there is an easy way to do this by using the Import CMSIS pack feature. 

Simply click on File>Import> select General then CMSIS Pack and Click on Next, as seen in the following figure.

CMSIS Pack.png

You will be asked to specify the pack file. Just use the browse button (...) to navigate to the location of the file and then click next. The pack file will be imported and made available. Easy!

Suitable Products
SSP