Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Extending beta license for the IAR EWARM-RS

Last Updated: 03/02/2016

Overview

In this simple guide you'll learn how to extend the beta license for IAR Embedded Workbench ARM RS and the IAR compiler.

Steps

Completing the following steps will extend IAR EWARM-RS beta license until 1st of July 2016.

Opening IAR License Manager

  • Begin by opening the start menu and navigating to:
    1. All programs
    2. IAR Systems
    3. IAR Embedded Workbench for ARM RS 7.40
  • ​Run the IAR License Manager

Note: If alternative directory path has been chosen during the installation, the steps above may be different.

Second Step

  1. Click License in the top menu.
  2. Select Check for License Renewal...
  3. In the pop-up window, select your EWARM-RS license.
  4. Click Check selected licenses.
  5. Once license expiration date is updated, press Renew selected.
  6. Verify that license has been extended in the Renewal Results window.

What's Next

You can now use the IAR EWARM-RS free of charge until July 2016.