Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How do I configure CS0 to work correctly with the external memory interface?

Latest Updated:09/19/2016

Question:

How do I configure CS0 to work correctly with the External Memory Interface on the DK-S7G2 and other kits?

Answer:

You can set the SDCLKout to off (it is on by default) in the clock configuration along with removing the bsp_sdram_init() call to use CS0.