Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How do I change the default HTTP port number at compile time?

Latest Updated:10/18/2016

Question:

How do I change the default port number for the HTTP server?

Answer:

You can change the default setting (of 80) of the HTTP server by making an edit to the define in nx_http_server.h:
#define NX_HTTP_SERVER_PORT 80 You need to also change this file to read only to keep it from being overwritten by the Synergy code generation process.
Suitable Products
SSP