Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How do Synergy MCUs simplify pin migration from device to device?

Latest Updated:10/13/2016

Question:

How do Synergy MCUs simplify the migration from one device to another while minimizing board layout impact?

Answer:

Synergy MCUs have a consistent pin-out when going from device to device. This allows smaller devices to fit into the same footprint as larger devices and makes it easy to add pins and traces when a larger device is needed. A PPT presentation showing the pin migration as attached below.

Synergy_pin_migration_plan_slides.pdf