Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is wear leveling for external QSPI memories supported within SSP 1.1.1?

Latest Updated:10/04/2016

Question:

Is wear leveling supported in SSP 1.1.1 for external QSPI Flash memories?

Answer:

Wear leveling is not supported for QSPI Flash devices as of SSP 1.1.1. Check current release notes and the SSP Users Guide to see if it is supported in future releases.