Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How do I implement an eMMC interface in SSP for a Synergy device?

Question:

How do I implement an eMMC interface in SSP for a Synergy device?

Answer:

Here is an example of an eMMC interface for the DK-S7G2 V3.1 kit.

Attached is a project for SSP 1.0 that works on my S7-DK V3.1 board. I have DIP switch S5 (on the main/top board) with DRAM(1) and JTAG(6) ON, all the others are off. S101 on the Baseboard SD(4) is ON, all the others are off. The project formats an SD card in the SD slot, creates a file and puts some text into it.

https://knowledgebase.renesas.com/@api/deki/files/413/S7_DK_SDCARD.zip