Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

sf_console Module Guide Resources

Last Updated:04/18/2017

Question:

Where can I find the references to module guide resources for the Console Framework module on sf_console?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Module Guide

The console framework module guide is targeted for SSP 1.2.0 and the SK-S7G2 Kit.

The console framework module guide describes what the sf_console module does, how to add it to your project, how to configure it, the associated APIs and provides an application project with a code walk through so you can quickly learn how to use the Console Framework module in your own design. We recommend that you have the SSP ISDE open and inspect the module stack, configuration information and code while reading over the application project description.

The most recent versions of the Console Framework module guide application note, application project and import guide will soon be available from the Synergy Gallery:  here

Module Guide Resources

  • The Developer Examples project uses the console framework to implement a complex multi-level menu and control interface to exercise the APIs for many Synergy modules. This project serves as a convenient 'bench' for testing and observing individual module API functions in operation. The Developer Examples are available as a project template in SSP 1.1.0 for the DK-S7G2. The associated application note is here: r11an0024eu0140-synergy-ssp-dev-ex.pdf

Know issues

  • No known issues as of posting date
Console Framework on sf_console module (SSP 1.2.0)