Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

USBX Host Class CDC ACM Module Guide Resources

Last Updated:03/01/2018

Question:

Where can I find the resources for the USBX Host Class CDC ACM module guide?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The USBX Host Class CDC-ACM module implements high-level APIs for USBX Host Class CDC-ACM applications and is implemented on g_ux_host_class_cdc_acm. The USBX Host Class CDC-ACM module configures the USBX Host Class CDC-ACM Source, USBX Host Configuration, USBX Source, USBX Port HCD, and a transfer driver. The USBX Host Class CDC-ACM module uses the DMAC/DTC and USB Host Class peripherals on the Synergy MCU.

 

Module Guide

The USBX Host Class CDC-ACM module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the USBX Host Class CDC-ACM module guide application note, application project and import guide are available here.

Module Guide Resources

The following useful user manuals are included in the X-Ware documentation package available here.

  • USBX Host Stack User’s Manual
  • USBX Device Stack User’s Manual

The following useful module guides and application projects are available from the Renesas web site:

  • USBX Device Class HID Module Guide- Application Project here.
  • USBX Device Class Mass Storage Module Guide- Application Project here.
  • USBX Device Class CDC-ACM Module Guide- Application Project here.
  • USBX Host Class HUB Module Guide- Application Project here.
  • USBX Host Class CDC-ACM Module Guide- Application Project here.
  • USBX Host Class Mass Storage Module Guide- Application Project here.

You can find all USBX Synergy projects and documents by searching for "USBX Synergy" on Renesas.com here.

 

Known issues

  • Refer to the SSP release notes for known issues, available here.

 

Suitable Products
SSP