Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Where do I find updates to the DK-S3A7 Kit information and examples?

Latest Updated:10/13/2016

Question:

Where do I find updates to the DK-S3A7 kit information, examples and issues?

Answer:

You can find all the updates to the DK-S3A7 kit information, examples and issues here.

1) What are the specifications for the LCD panel used on the DK-S3A7 V2 Kit?

You can find a Knowledge base article with the information here: 

What are the specifications for the DK-S3A7 V2 LCD Panel?

2) What are the correct switch settings to enable JTAG on the DK-S3A7 V2 kit?

What are the JTAG switch settings for Synergy kits to enable debugging?