Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

r_sdadc Module Guide Resources

Last Updated:02/27/2018

Question:

Where can I find the references to module guide resources for the Sigma Delta Analog to Digital Converter HAL module on r_sdadc?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The SDADC HAL module implements the ADC API for analog-to-digital conversions on r_sdadc. It supports the SDADC24 24-bit analog-to-digital converter peripheral available on the Synergy microcontroller hardware. A user-defined callback can be created to process the data each time a new sample is available.

This module supports the following features:

  • 24-bit sigma delta A/D Converter
  • Single scan or continuous scan operation mode
  • Single-ended or differential input
  • Gain of up to 32 on differential inputs
  • Oversampling ratio configurable on differential inputs

 

Module Guide

The module guide is not yet available.

 

Module Guide Resources

There are currently no resources available for this module.

 

Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
SSP
  • Was this article helpful?