Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

r_slcd Module Guide Resources

Last Updated:11/27/2017

Question:

Where can I find the references to module guide resources for the Segment LCD Controller module on r_slcd?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Segment LCD HAL module uses the Segment LCD Controller (SLCDC) to display data on a Segment LCD. The driver initializes the LCD for displaying data and configures the drive- voltage generator, the display waveform, the number of time slices, and the bias methods to drive the LCD. This module provides functions to display data to a specified set of segments, to update existing segment data, to enable and disable display, to set the display area, and to adjust the contrast.

This module supports selecting the following features:

  • Internal voltage- boosting for the LCD driver voltage generator: select the capacitor split method or the external resistance division.
  • Display bias: select the 1/2 bias method, 1/3 bias method, or 1/4 bias method.
  • Time slice of the display: select static, 2-time slice, 3-time slice, 4-time slice, or 8-time slice.
  • Display waveform: select waveform A or waveform B.
  • Display data area: select A-pattern, B-pattern, or blinking. You can switch the display data area.
  • Use the RTC periodic interrupt (PRD) to generate a blinking display with A-pattern and B-pattern.
  • Adjust the reference voltage (which is generated when operating the voltage boost circuit) in 16 steps (contrast adjustment.)

Module Guide

The Segment LCD HAL module guide is targeted for SSP 1.2.0 and above and the SK-S7G2 Kit.

The most recent versions of the Segment LCD HAL module guide application note, application project and import guide are available  here

Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • DK-S3A7 v.2.0 Out-of-Box Demo Programming Guidelines - Application Project  here.
  • Renesas Synergy™ Project DK-S3A7 Segment LCD Display Example here.

Known issues

  • Refer to the most recent release notes for known issues, available here.
Suitable Products
SSP